July 17, 2015

The BBC micro:bit and why it’s important #STEM

Driving the micro:bit legacy The micro:bit project is a groundbreaking partnership between international corporations, including Freescale, which provided a Kinetis KL26 […]
July 15, 2015

Why Companies Should Identify with Identity Protection

If there was one take-away from this year’s MWC it’s this: mobility large or small is unthinkable without discussing privacy […]
July 10, 2015

Micro:bit Unveiled

Announced in March this year, the BBC’s micro:bit has been unveiled today.  All the people excited by this fantastic initiative […]
June 25, 2015

Smart loyalty: MIFARE drives the next trend in retail

The modern loyalty program, which rewards customers for their business, can be traced back to the early 1980s, when airlines […]
June 18, 2015

Motors & MCUs – The hidden heroes of the modern home

Without motor control, our homes and lives would be far less convenient than they are today – we’d still be […]
June 9, 2015

Robust parts for Harsh Environments, NXP’s Automotive Logic Parts Lead the Way

Automotive applications present a harsh environment for semiconductor components. Parts in these applications must continue to work reliably, despite operating […]
April 28, 2015

Welcome home to the 21st century

Our world is full of technological marvels that have enhanced many aspects of our lives. The unabated rise of the […]
April 23, 2015

Mining sensor data, Part 3 (Capturing to a file)

In Creating a Data Logger embedded application using the Intelligent Sensing Framework (ISF 2.1), my colleague Dave Munsinger introduced the Intelligent […]
April 23, 2015

Performance and efficiency – a timeless quest with evolving requirements

Performance and efficiency are the central pillars that define the entire microprocessor business. The “Holy Grail” has always been to […]
Buy now