How Automotive Ethernet Delivers: The Data Dilemma Of Highly Autonomous Vehicles

How Automotive Ethernet Delivers: The Data Dilemma Of Highly Autonomous Vehicles

At NXP, we see automotive Ethernet in the distributed vehicle network as the best solution for automotive data management. It enables broad connectivity and provides the required low latency and quality of service needed for advanced control functions and full-motion video. It also reduces weight, saves power, increases efficiency, enables upgrades and makes autonomous driving more affordable.

Ethernet provides high bandwidth for higher levels of data processing
With an automotive Ethernet network, multiple vehicle systems simultaneously have access to high bandwidth over a single Unshielded Twisted Pair (UTP) cable. Ethernet then becomes the backbone of the vehicle, able to support higher levels of data processing and different communication types. Using traffic engineering features like Time Aware Shapers, each port receives a dedicated bandwidth and the entire backbone is capable of IP connectivity. Collaboration across the industry through the OPEN Alliance SiG is pushing further innovation in automotive Ethernet. The alliance looks to drive non-proprietary industry standards to enable the migration from multiple closed applications to an open, scalable Ethernet based network.

NXP supports 100BASE-T1, the latest spec for automotive Ethernet
The latest specification for automotive Ethernet is the 100BASE-T1 – this is the first automotive baseband medium for 100 Mbps Ethernet over single UTP cables. It follows the IEEE 802.3bw standard with PHY layer specs for point-to-point full duplex on 100 Mbps operations.

NXP actively supported the development of this standard. The expansion of our automotive Ethernet portfolio is testament to our commitment to improving the network capabilities for car makers. The new TJA1102 Ethernet PHY provides innovative sleep and wake-up-forwarding functionality, so that the same Ethernet channel provides data transmission and wake-up of the ECU, saving the additional wire that otherwise would be required. This dual port PHY is the first in the industry designed to 100BASE-T1, and meeting the OPEN SiG Standard for Sleep and Wake-Up, also known as OPEN TC10. It includes two transceivers in a small 8 mm x 8 mm package that results in more than 30% area saving compared to two single port PHY devices.

The TJA1102 dual port PHY is combined with the latest SJA1105x Ethernet switch to form a highly optimized Ethernet subsystem. The SJA1105x is a five port Gigabit switch that streamlines the design of safety-related ECUs such as ADAS and gateways. It is the industry’s first ASIL-A compliant Ethernet Switch, certified by NXP’s own SafeAssure functional safety program. It is equipped with extensive TSN capabilities for time-aware shaping technology that is prepared to manage the data flow of increasingly complex future vehicle networks.  This is particularly important if you consider how networks are developing. With the move towards the Ethernet backbone where there might be a central compute node with a zonal distribution of gateways with switches. This means that the network architecture will be optimized for reduced wiring and at the same time provides a standardized, scalable architecture that increases processing and security capabilities.

Handling increasing data transfer rates
One of the key challenges in making the move towards this will be the ability to cope with further increasing data transfer rates. Typically, this topology will require an increase from 1 Gbps to 10 Gbps to still enable data aggregation over the backbone, which puts a considerable strain not only on the networking components, but also on the software architecture. Today, in the standard Linux® OS environment, there is already 100% load on both the transceiver and receiver cores. To be able to increase the data transfer rate needed to scale up to 10 Gb, standard OS APIs are not effective for high packet rates. Instead, data path centric software architectures and implementations will have to be used to accommodate the hardware acceleration, which is needed for 10 Gb.

Today, Ethernet is still in the early phases of deployment, with a fast maturing ecosystem. Already automakers are making the move towards these optimized subsystems for their entry level volume produced vehicles, but without further standardization and industry-wide collaboration there could be a significant challenge to meeting the requirements for the super-high-performance computing of the autonomous car of tomorrow.

 

Guenter Sporer
Guenter Sporer
Guenter Sporer is Director of Marketing, Systems and Application Engineering for NXP’s Automotive Ethernet Solutions group. He successfully launched NXP’s first automotive Ethernet product family of 100BASE-T1 PHYs and AVB/TSN switches and, together with his team, is responsible for all aspects of defining NXP's next generation high-speed networking solutions. Guenter also represents NXP in the OPEN Alliance Steering Committee.

Comments are closed.

Buy now