January 7, 2020

Microsoft and NXP: A Powerhouse Collaboration for Advanced Voice Command in a Smarter More Connected World

With voice command rapidly becoming an indispensable part of navigating every aspect of daily life, NXP recognized early on the […]
January 6, 2020

NXP Smarter World Podcast | The Changing Role of Vehicle Networks

The vehicle data revolution is fully underway. More and more vehicles are connected. Some already have upwards of 40 sensors […]
January 6, 2020

Collaboration is Critical for Real-World Validation of Autonomous Vehicles

The road to automated driving has definitely seen a few bumps! However, with the sobering statistic of approximately 1.3 million […]
January 6, 2020

Open Software Helps Fuel Autonomous Vehicle Innovation

Deploying safe, autonomous vehicles at scale is a colossal undertaking that requires much stronger synergies between corporate development, government participation […]
January 6, 2020

The Future Is Now! i.MX 8M Plus Leading Machine Learning to the Edge

Sci-fi movies and TV shows have long covered the future of artificial intelligence including popular characters such as The Robot […]
January 6, 2020

Why Add an ISP and Machine Learning Acceleration to the i.MX 8M Family

NXP likes to do things differently – to lead and innovate. We’ve being successfully supporting camera modules interfaces on i.MX […]
December 9, 2019

Introducing The Newest Player in Edge Computing – The i.MX 8M Nano and Board Partners

The i.MX 8M Nano applications processor follows the highly successful i.MX 8M Mini into the world of edge computing with […]
December 6, 2019

20 Years of Wi-Fi: On the Way to Wireless Freedom – Part I

You can’t see it, touch it, or hear it – yet Wi-Fi® has had a tremendous impact on the modern […]
December 6, 2019

20 Years of Wi-Fi: On the Way to Wireless Freedom – Part II

This is the second instalment in a series of blogs covering the history of Wi-Fi®. This part will look at […]
Buy now