September 7, 2018

The Anatomy of Smart Pharma: IoT connected NFC Tags for Patient Engagement & Protection

These are interesting times for pharmaceutical companies. On the one hand, various market analysts, including Deloitte Global Life Sciences, are […]
October 17, 2017

Preventing prescription drug misuse: how smartcards can help contain the opioid epidemic in the US

According to data compiled from hundreds of health agencies in the US, drug overdoses took the lives of more than […]
April 26, 2017

It’s All About the Right Tag!

Let’s start with a confession; I’m part of the statistics. My immune system is quite fragile, providing a playground for […]
November 18, 2015

6 ways NFC helps healthcare

Of the many industries using Near Field Communication (NFC) to add convenience, increase efficiency, and automate processes, healthcare is gaining […]
July 16, 2014

The wearable revolution has already begun

There is plenty of discussion these days about ‘wearable technology’, and many consumer electronics companies have ventured into the market […]
October 1, 2013

Mobile health market primed for major growth

The past few weeks have seen a throng of mobile health announcements that show the market is growing rapidly in […]
October 31, 2012

The Future of Healthcare? Technology Detects Cancer in Blood

Interesting read about technology and healthcare as part of the Asian Innovation Awards 2012, in The Wall Street Journal. As part of […]
Buy now