February 25, 2020

Machine Learning Acceleration – The Race to the Top and the Bottom

Many application developers are still comprehending the benefits of machine learning (ML), but one thing is clear – machine learning […]
January 6, 2020

The Future Is Now! i.MX 8M Plus Leading Machine Learning to the Edge

Sci-fi movies and TV shows have long covered the future of artificial intelligence including popular characters such as The Robot […]
January 6, 2020

Why Add an ISP and Machine Learning Acceleration to the i.MX 8M Family

NXP likes to do things differently – to lead and innovate. We’ve being successfully supporting camera modules interfaces on i.MX […]
December 9, 2019

Introducing The Newest Player in Edge Computing – The i.MX 8M Nano and Board Partners

The i.MX 8M Nano applications processor follows the highly successful i.MX 8M Mini into the world of edge computing with […]
December 4, 2019

Meet the i.MX 8M Nano

NXP’s latest quad-core applications processor for secure, affordable and intelligent edge computing has landed. Built on the success of the […]
November 20, 2019

NXP Solves Vulnerability Detection Challenge for Developers with New Automated Tool

According to VXCHNGE, there will be 20.4 billion IoT devices by 2020. That is a staggering number, no doubt! But […]
October 8, 2019

Unlock eCockpits and Camera Monitoring Systems with i.MX 8QuadMax Ecosystem Partners

True integrated eCockpits for cars, multi-camera monitoring in industrial systems and multi-domain systems requiring both open access and safety/security are […]
October 2, 2019

An Order of Magnitude: Launching the Gigahertz MCU Era

Over time, advancement for general purpose microcontrollers has essentially been… incremental. Traditionally, microcontrollers are built in older, lower cost wafer […]
August 22, 2019

Applications Processing at MCU-Level Low Power

Let’s get started with i.MX 7ULP The i.MX 7ULP crossover applications processors, NXP’s first 28nm FDSOI applications processors for the […]
Buy now