NXP is a top 100 Global Innovator: Big deal?

NXP is a top 100 Global Innovator: Big deal?

This week, it was announced that NXP was included in the list of 2016 Top 100 Global Innovators compiled by Clarivate Analytics. What does this actually mean? Is it really a special distinction or just another list? Just how it is decided who makes the grade?

Clarivate Analytics is the former Intellectual Property & Science business of Thomson Reuters. Six years ago, it started compiling and publishing a Top 100 Global Innovators list. The ranking includes global companies and institutes based on a thorough study of their patenting performance.

These criteria make sense, because true innovation requires unique solutions and discoveries. An associated patent, granted by an independent patent office, is legal recognition of the uniqueness of an invention. It also protects the owner from infringement by others.

The number of patent applications by a company is a good indication of how innovative it is. It’s not the only one, however, as not every application is granted. For example, many applications are not approved because another party has already applied for a patent for the invention, or because it is simply not unique enough.

The most relevant consideration for the researchers at Clarivate Analytics is how many patent applications a company has submitted, as well as the number that is actually granted.

The recent merger with Freescale obviously helped to increase our patent volume, but there are two more criteria to qualify for the Top 100.

Applying for a patent is costly and requires a lot of effort. If an invention has a lot of commercial potential, then it’s worthwhile to submit various patent applications to different national patent offices worldwide in a coordinated way. This way of protecting an invention in major world markets is an indication of an invention’s potential business value, and it is used as a third criterion for the Top 100 ranking.

In order to measure the global influence of a patent, it is useful to look at the number of times it was cited by other companies when applying for patents for their own inventions. By citing earlier patents, a company can describe how their invention builds further on previous innovations by others. The more often a patent is cited, the more influential it is in a particular field of expertise and in associated markets.

In summary, being ranked among the Top 100 Global Innovators is not just based on the number of granted patents, but also on the commercial impact of the inventions involved. This is in accordance with one of the definitions of innovation: “Innovation is Invention times Market Acceptance.”

In 2015, the Top 100 innovators spent more than $227 billion on R&D and generated more than $4 trillion in revenue. That’s over 5.5% of sales spent on R&D. In semiconductors, the R&D/Sales rate is even higher, roughly 15%, or around $1.5 billion annually at NXP. We need a very high return on that investment to be successful in our business. Therefore we need to invest in inventions and developments that help us create a competitive advantage. A strong patenting strategy and patent portfolio is a key success factor to achieve that.

Being recognized by a prestigious organization like Clarivate Analytics as a Top 100 Global Innovator is acknowledgement of the powerful position we have achieved. It contributes to our reputation as an innovative front-runner and makes us a more attractive partner, supplier, and employer.

Surely that’s something we can all be proud of!

Chris Hardingham
Chris Hardingham
Chris heads a global team of patent attorneys, with responsibility for NXP Semiconductors' patent portfolio. NXP produces many hundreds of cutting-edge inventions every year. Chris' department determines which inventions should form part of our Patent Portfolio, in line with our goals, strategy and budgets. The group also manages the drafting of the Patent Applications, to meet strict legal, technical and linguistic requirements. It also handles the negotiation with National Patent Offices. Chris enjoys interaction at all levels of the business from first-time inventors to the senior business leaders, and practicing his profession in front of the European Patent Office.

Comments are closed.

Buy now