Continuous Strong Growth Makes NXP UCODE the #1 RAIN RFID Tag IC

Continuous Strong Growth Makes NXP UCODE the #1 RAIN RFID Tag IC

The first quarter of 2019 proved to be another strong one for NXP’s portfolio of RAIN RFID ICs. Not only did we ship more than two billion UCODE ICs, we also confirmed our number-one position for RAIN RFID tag IC revenue.

UCODE 8 Performance Drives Growth

NXP’s ongoing success with RAIN RFID tags can be credited to the best-in-class performance of our latest implementation of the RAIN RFID architecture, UCODE® 8, which enables quick programming and fast, highly accurate inventory counts. What’s more, UCODE 8 ICs consume 20% less power than competing solutions. The combination of high performance and low power consumption makes it possible to do faster, more reliable inventory counts and to manage items more easily in the supply chain.

UCODE 8 also enables smaller designs and at the same time, brings tagging capabilities to smaller, previously difficult to tag retail items such as cosmetics and food.

RAIN RFID Continues to Expand

The strength of NXP’s UCODE 8 portfolio also reflects strong growth for RAIN RFID overall. The RAIN RFID Alliance, the industry organization that promotes adoption of RAIN RFID technology, reports that volume from RAIN RFID tag ICs grew 23% from 2017 to 2018, and they believe the market is on track to exceed 20 billion tag shipments annually for 2020 and beyond. Key applications, including retail apparel and footwear, airline baggage tagging, and logistics services, will help drive this growth.

RAIN RFID Powers the IoT

RAIN RFID tags can be found across the Internet of Things (IoT), where they create a link between an exceptionally broad range of items and the cloud. RAIN RFID tags work without batteries and support batch reading, without direct line of sight. Tags can be attached or embedded, flexible or hardened, and can store just basic identification numbers or be outfitted with password-protected memory to store additional information. They can work on their own, as item identifiers, or can easily combine with sensors, to track things like temperature or humidity. RAIN RFID tags also come with high-end security features, in the form of crypto authentication, which protects tag identities from cloning and which ensures secure protection of the stored data.

NXP’s Technology

NXP’s UCODE 8 family supports a 16-bit identifier and enables insertion of the Brand ID during production, so the ID can be locked before shipment. The Brand ID is located in a separate, undisclosed memory location, for added protection from unauthorized access. University of Auburn-certified inlays using NXP’s UCODE ICs are available in close to 30 different formats, and growing, so it’s easy to find the right configuration for a given application.

To experience the power of UCODE 8 RAIN RFID, be sure to vistit us at GS1 Connect (NXP booth #38) between June 19-21 in Denver, CO. For more information visit nxp.com/rfid or email us at rfid.info@nxp.com.

Ralf Kodritsch
Ralf Kodritsch
Ralf Kodritsch is Director Marketing for RAIN RFID Solutions at NXP Semiconductors. He has over 20 years of experience in the semiconductor industry and more than 12 years of experience in the RFID industry, thereby built up a vast industry network and profound market insights. His vast industry network and profound market insights are key to providing best-in-class solutions and services to the RAIN RFID Industry. His vision is to make RAIN RFID ubiquitous in our everyday life, for the benefit of the consumers and businesses alike.

Comments are closed.

Buy now