NXP and Microsoft Announce Public Preview of Windows 10 IoT Core on i.MX 6 and i.MX 7 Applications Processors

NXP and Microsoft Announce Public Preview of Windows 10 IoT Core on i.MX 6 and i.MX 7 Applications Processors

Earlier this year, NXP and Microsoft announced a private preview of Windows 10 IoT Core on NXP i.MX6 and i.MX7 applications processor silicon. Hundreds of participants expressed their interest in the combination of 10 years of Windows security updates and the flexibility and reliability of NXP silicon.

During the preview, Microsoft and NXP engineers spent thousands of hours tuning and improving the board support package (BSP) based on input from the hundreds of commercial customers evaluating the solution. NXP and Microsoft worked with customers interested in modernizing legacy industrial controllers, building automation solutions, and gateways with class-leading security such as trusted I/O.

Interest in the private preview exceeded the capacity of the program and today, we are announcing the promotion of the i.MX6 and i.MX7 BSP to a non-commercial public preview. Because of the long history Microsoft and NXP have in the embedded and IoT markets, we understand the need for design flexibility. Therefore, in addition to the multiple single board computers and system-on-module solutions Microsoft, NXP, and our hardware partners have enabled, the i.MX 6 and i.MX 7 BSP is provided under open source licensing. Now, everyone will be able to access the complete BSP content for the i.MX6 and i.MX7 product families for evaluation use on their hardware along with the October 2018 release of Windows 10 IoT Core. To get started, please go to http://aka.ms/iotnxp. We are excited to see what you will make.

A public preview for the i.MX 8M family and a commercial release of the i.MX 6 and i.MX 7 BSP will be available in the future.

 

 

 

 

Pat Stilwell
Pat Stilwell
Patrick Stilwell is a Product Line Manager for i.MX applications processors and has over 20 years of experience in the semiconductor industry from manufacturing and new product introductions to product management. He specializes in all product management disciplines in support of customer program enablement.

Comments are closed.

Buy now