Unlock eCockpits and Camera Monitoring Systems with i.MX8QuadMax Ecosystem Partners

Unlock eCockpits and Camera Monitoring Systems with i.MX8QuadMax Ecosystem Partners

True integrated eCockpits for cars, multi-camera monitoring in industrial systems, and multi domain systems requiring both open access and safety/security are transforming the way we interact. To operate these complex systems, we need multiple high definition displays, running multiple operating systems, enabled with new seamless HMI, with safety systems such as application sand-boxing. The NXP i.MX 8QuadMax offers the potential to deliver all these features in one applications processor.

As the processor’s capabilities expand, so can the complexity of getting your product to market. To help with this, NXP delivers the chip, AND puts an ecosystem of partners in place, to enable a wider range of customers to develop a faster with the i.MX 8QuadMax processor.

Today, we are announcing a select group of early-access partners that NXP has been working with to develop an active worldwide ecosystem for the i.MX 8QuadMax processor. Customers are encouraged to engage immediately to leverage the expertise of all these partners; below is a summary of how they describe their development plans:

  • BCM Advanced Research is developing a system-ready single board computer and SMARC module aimed at the medical, infotainment and retail markets.
  • Artesyn will offer a flexible PCIe card and a suite of software development tool for simple image processing solutions.
  • Variscite is developing both a system-on-module and single board computer solution designed to deliver the best cost/performance, production-ready software and longevity.
  • PHYTEC will utilize the i.MX 8 processor to enable rapid prototyping, agile development services and Industry 4.0 manufacturing.
  • iWave Systems is developing a SOM for high performance graphic-intensive applications such as computer vision, 4K signage, vehicle infotainment, video analytics and gaming consoles.
  •  The Advantech Embedded Computing Group will develop the ROM-7720 SOM module for imaging, machine vision, audio, voice, video and safety critical applications.
  • Toradex extends its pin-compatible Apalis Computer Module family with the i.MX 8 family. It will fully benefit from Toradex ecosystem and free support.
  • Congatec is designing a rugged conga-QMX8 Qseven computer-on-module that will deliver an application ready computing core to connect the industry 4.0.

These partners, along with NXP, will be at Embedded World in Nuremberg, Germany from March 13-16. NXP will be showcasing the capability of the i.MX 8QuadMax applications processor, so please stop by our booth 4A-220 to see its capabilities, and visit our partners’ booths to learn some exciting ways they plan to enhance the i.MX 8QuadMax ecosystem.

 

Robert Thompson
Robert Thompson
Robert Thompson is chief enablement architect for i.MX applications processors. He focuses on developing the ecosystem to enable customers to get to market as fast and competitively as possible. Robert is an industry expert in consumer electronics with over 20 years of experience in diverse regions, including Europe, Brazil and the US.

Comments are closed.

Buy now